Button widget text wrap

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Button widget text wrap

跳至解决方案
5,943 次查看
mitchkapa
Contributor III

Is it possible to have the text within a button widget wrap to appear on multiple lines?

0 项奖励
回复
1 解答
5,917 次查看
david_piskula
NXP Employee
NXP Employee

Hello @mitchkapa,

it's definitely possible but requires manual changes to the code after you've generated it.

This is the way a label is added to a button "setup_scr_screen.c":

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

In order to enable wrapping you need to do two things.

  1. Manually edit the width of the label inside the button: lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90)); - the lv_pct(90) value sets the width to 90% of the width of the parent (meaning the button in this case). You can also use an absolute value, like 200. By default it seems that LVGL sets the width to fit the whole text in the label and doesn't take the button width into consideration, which means that the label is created as wider than the button even though it's inside the button and simply enabling wrapping won't have any effect.
  2. Choose the long text behavior: lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90));
	lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

I will suggest to add this functionality inside Gui Guider so that people don't have to manually edit it every time. Thanks for the question!

IMG_20220808_104454.jpg

 

Best Regards,

David

在原帖中查看解决方案

3 回复数
5,909 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @mitchkapa 

We have escalated it as a GUI Guider feature request.

Thanks for bringing the problem to our attention.

BR

Jun Zhang

5,918 次查看
david_piskula
NXP Employee
NXP Employee

Hello @mitchkapa,

it's definitely possible but requires manual changes to the code after you've generated it.

This is the way a label is added to a button "setup_scr_screen.c":

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

In order to enable wrapping you need to do two things.

  1. Manually edit the width of the label inside the button: lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90)); - the lv_pct(90) value sets the width to 90% of the width of the parent (meaning the button in this case). You can also use an absolute value, like 200. By default it seems that LVGL sets the width to fit the whole text in the label and doesn't take the button width into consideration, which means that the label is created as wider than the button even though it's inside the button and simply enabling wrapping won't have any effect.
  2. Choose the long text behavior: lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90));
	lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

I will suggest to add this functionality inside Gui Guider so that people don't have to manually edit it every time. Thanks for the question!

IMG_20220808_104454.jpg

 

Best Regards,

David

5,898 次查看
mitchkapa
Contributor III

Thanks!

0 项奖励
回复