Button widget text wrap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Button widget text wrap

ソリューションへジャンプ
5,942件の閲覧回数
mitchkapa
Contributor III

Is it possible to have the text within a button widget wrap to appear on multiple lines?

0 件の賞賛
返信
1 解決策
5,916件の閲覧回数
david_piskula
NXP Employee
NXP Employee

Hello @mitchkapa,

it's definitely possible but requires manual changes to the code after you've generated it.

This is the way a label is added to a button "setup_scr_screen.c":

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

In order to enable wrapping you need to do two things.

  1. Manually edit the width of the label inside the button: lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90)); - the lv_pct(90) value sets the width to 90% of the width of the parent (meaning the button in this case). You can also use an absolute value, like 200. By default it seems that LVGL sets the width to fit the whole text in the label and doesn't take the button width into consideration, which means that the label is created as wider than the button even though it's inside the button and simply enabling wrapping won't have any effect.
  2. Choose the long text behavior: lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90));
	lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

I will suggest to add this functionality inside Gui Guider so that people don't have to manually edit it every time. Thanks for the question!

IMG_20220808_104454.jpg

 

Best Regards,

David

元の投稿で解決策を見る

3 返答(返信)
5,908件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @mitchkapa 

We have escalated it as a GUI Guider feature request.

Thanks for bringing the problem to our attention.

BR

Jun Zhang

5,917件の閲覧回数
david_piskula
NXP Employee
NXP Employee

Hello @mitchkapa,

it's definitely possible but requires manual changes to the code after you've generated it.

This is the way a label is added to a button "setup_scr_screen.c":

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

In order to enable wrapping you need to do two things.

  1. Manually edit the width of the label inside the button: lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90)); - the lv_pct(90) value sets the width to 90% of the width of the parent (meaning the button in this case). You can also use an absolute value, like 200. By default it seems that LVGL sets the width to fit the whole text in the label and doesn't take the button width into consideration, which means that the label is created as wider than the button even though it's inside the button and simply enabling wrapping won't have any effect.
  2. Choose the long text behavior: lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);

 

	ui->screen_btn_1_label = lv_label_create(ui->screen_btn_1);
	lv_label_set_text(ui->screen_btn_1_label, "very very very very very very very long text wrapped with LV_LABEL_LONG_SCROLL");
	lv_obj_set_width(ui->screen_btn_1_label, lv_pct(90));
	lv_label_set_long_mode(ui->screen_btn_1_label, LV_LABEL_LONG_WRAP);
	lv_obj_set_style_pad_all(ui->screen_btn_1, 0, LV_STATE_DEFAULT);
	lv_obj_align(ui->screen_btn_1_label, LV_ALIGN_CENTER, 0, 0);

 

 

I will suggest to add this functionality inside Gui Guider so that people don't have to manually edit it every time. Thanks for the question!

IMG_20220808_104454.jpg

 

Best Regards,

David

5,897件の閲覧回数
mitchkapa
Contributor III

Thanks!

0 件の賞賛
返信