Arduino IDE and LGVL Function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Arduino IDE and LGVL Function

1,879 次查看
allacmc
Contributor I

I would like to export the GUI BUILDER files and use them in the Arduino IDE.

Which lvgl function do I call to initialize the app made in the GUI Builder?

What files do I have to change considering that in the Arduino IDE I need to have all the files in the same directory without folders and subfolders?

Could anyone help me in this regard?

0 项奖励
回复
1 回复

1,825 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that it is a large project to port the LVGL to Arduino IDE.

BR

XiangJun rong

0 项奖励
回复