Arduino IDE and LGVL Function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Arduino IDE and LGVL Function

1,863 Views
allacmc
Contributor I

I would like to export the GUI BUILDER files and use them in the Arduino IDE.

Which lvgl function do I call to initialize the app made in the GUI Builder?

What files do I have to change considering that in the Arduino IDE I need to have all the files in the same directory without folders and subfolders?

Could anyone help me in this regard?

0 Kudos
Reply
1 Reply

1,809 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that it is a large project to port the LVGL to Arduino IDE.

BR

XiangJun rong

0 Kudos
Reply