GUI Guider Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI Guider Knowledge Base

Discussions

Sort by:
Designing modern, responsive embedded graphical interfaces has never been easier. In this article, we share the complete set of resources from our hands‑on lab focused on building GUIs with NXP GUI Guider and the LVGL graphics engine, using the FRDM‑MCXN947 development board. This guide will help you import the E‑Bike demo, customize screens and events, simulate your UI, and deploy it directly on hardware. 
View full article
GUI Guider 1.8.1 Just released!   This version integrates your NXP account to enhance user experience in content delivery. The new version also improves FreeMASTER integration enabling variable binging to the widgets, and much more:   - EV Charger example application - Widgets and screen statistics - Video player for i.MXRT1160/70 - Yocto Linux BSP upgrade to 6.6.23-2.0.0   Try it on your own https://www.nxp.com/GUI-GUIDER     New IDE function NXP SSO login Seamless simulator run in FreeMASTER Unify generated code style EV charger demo Widgets and screens statistic License change   UX/DX improvement Retry mechanism of read FreeMASTER variable Update the widgets search window expand style Highlight selected image in image window Add the copy event target Add the event trigger editor   SDK and targets Add 800x400 resolution for MultiLanguage and Aircon. Enable video for I.MX RT1160/70 i.MX91 11x11 Upgrade toolchain Upgraded to Linux BSP to 6.6.23-2.0.0 Remove landscape mode of 1280x720 for I.MXRT 1160/11170 Allow input details for ‘other’ option for Survey
View full article
The newest version of GUI Guider comes with UI and functionality improvements. It is extended by new widgets and tuning options. Also, stability and performance were improved. Let's see the significant updates:   - LottieFiles animations (https://lottiefiles.com/) - MCX N and LPC5506 added - Resource manager utilized - Complex Image Tool - and much more   Try it on your own at https://www.nxp.com/GUI-GUIDER  
View full article
Newest release comes with many usability and performance improvements. Some highlights amongst the improvements include: LVGL supported updated to v8.2.0 RT-Thread RTOS support Custom GUI resizing Concept of design style Batch image import New themes Widget shadows Easy widget aligning Screen and image preview And much more… We’ve also added support for LPC54628 external flash storage, landscape mode for i.MX RT1170 and the RK055HDMIPI4MA0 display. https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER
View full article
New release of GUI Guider v1.1, the user-friendly graphical user interface development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library.
View full article
The latest version introduces an enhanced project creator, unlocking new possibilities for seamlessly combining boards and predefined templates making application creation easier and more intuitive than ever before. Exciting news also for motor-control enthusiasts - GUI Guider now features advanced motor parameter configuration options, bringing greater flexibility and precision to your development workflow. - New demo - Heterogenous multicore for Real-Time Edge framework - FRDM-IMX91S, i.MX943, i.MX95 - Terminal debug support - GUI xTurbo performance optimizations Try it on your own! https://www.nxp.com/GUI-GUIDER
View full article
HO! HO! HO! GUI Guider 1.10.1 is out now! This version comes with significant ecosystem update including LVGL 9.3.0 and G2D graphics acceleration support for Application processors. Stability and performance were improved also as more platforms integrated. Check out major improvements: - G2D acceleration - multi-touch support including demo - i.MX RT700-EVK - Zephyr 4.2 Try it on your own! http://nxp.com/gui-guider
View full article
Dear developers, GUI Guider has new version now! In this version, we’ve introduced major updates designed to deliver a more powerful and efficient development experience. Whether you’re working in industrial control, smart home or consumer electronics, these updates will breathe new life into your projects! Key Updates: Support more characters in project name hyphens (-) and at signs (@) are supported in project names from this version. Currently the allowed characters include letters, numbers, underscores (_), hyphens (-), and at signs (@). Custom folder path for code generation Support customizing the path of generated directory, eliminating manual copying operations and improving project development efficiency. Code editor autosave custom code Don't worry about forgetting to save custom code anymore! The new version automatically saves custom code for you. Image converter supports more functions (LVGL v9) Dither mode and stride automatic alignment functions are supported in LVGL v9 image conversion tool. dither mode optimizes the display effect of images, The combination of stride automatic alignment and VGLite GPU further enhances application performance. Industrial demo on MCX: agriculture control Add agricultural control templates that can run smoothly on the FRDM-MCXN947 target board, helping you quickly build a professional industrial control interface. Add Camera and Video support for i.MX 93 (LVGL v9) Camera and Video are supported for i.MX 93 EVK and FRDM-IMX 93 boards. users can develop their multimedia applications refer to the provided demos. New Target boards The version has added support for development boards such as FRDM-IMX91 (LVGL v9) and FRDM-RW612 (LVGL v9), expanding hardware compatibility and meeting more development needs. Add benchmarking demos (LVGL v9) Smart clock demo is added for i.MX RT700 to showcase the powerful graphics acceleration capabilities of VGLite GPU. FlashingImages and LVGLBenchmark demos are added for i.MX RT1060-EVKC to demonstrate the optimization of rendering speed. Why do you choose GUI Guider? Minimalist design and efficient development GUI Guider offers an intuitive drag-and-drop interface design tool, enabling rapid generation of high-quality LVGL code without complex programming. This significantly boosts development efficiency, allowing you to focus on creativity and functional implementation. Keeping up with the latest technology and strong compatibility We continuously add support for the latest hardware platforms and operating systems, ensuring your projects remain at the forefront of technology while effortlessly addressing diverse requirements. Rich examples and templates Whether for industrial applications, smart home appliances, or IoT devices, GUI Guider provides a variety of demos and templates to help you get started quickly, shortening the development cycle from concept to finished product. Get the new version now! Let’s download the latest GUI Guider now and experience these powerful new features! Whether you are a novice or a seasoned developer, GUI Guider will be your reliable assistant on the path of HMI development. Download link:Get GUI Guider 1.9.1 now Video tutorials:GUI Guider Academy Official website:Visit NXP official website Feedback:Community forum Follow us for more development tips and the latest news! GUI Guider, Make graphical interface development easier!
View full article
GUI Guider 1.8.0 is out now! This version comes with the new UI visualizer for Events creation that brings better events flow in your application! Stability, widgets and tool appearance were improved also and much more: - Project export to HTML - Updated example applications - Improved code editor - Added FRDM-MCXN236 - Portrait mode for MCX-FRDM - Removed LVGL v7 Try it on your own https://www.nxp.com/GUI-GUIDER
View full article
The newest version comes with a video converter tool that easily converts video to animation. Now you can play videos on low-resource devices. Also as UI was significantly improved to bring better user experience and ease of use. Among other improvements, GUI Guider comes with a new demo application covering very popular two-wheelers.   Try it on your own at https://www.nxp.com/GUI-GUIDER
View full article
GUI Guider 1.7.0 is out now!   This version brings many changes. One of them is the collaboration of the two most popular MCU tools. GUI Guider now integrates FreeMASTER support. Real-time tuning, especially of motor control applications, is now much more user-friendly. Next, the GUI Guider is expanded to support the latest FRDM-MCXN947 development kits along with the new IPS display from NXP LCD-PAR-S035.     Try it on your own at https://www.nxp.com/GUI-GUIDER   https://www.nxp.com/FRDM-MCXN947 https://www.nxp.com/FREEMASTER https://www.nxp.com/design/design-center/development-boards/...
View full article
  Do you want to try a bigger screen? The new version supports the RPi 7" panel directly connected to i.MX RT1170-EVKB. MPU fans will be also satisfied by adding the QNX operating system for i.MX93 platform! Don't miss major updates: - Smart Watch Demo - enhanced support for round displays - new platforms added - more widget customization options - and much more Try it on your own at https://www.nxp.com/GUI-GUIDER
View full article
📣 Try out the new GUI Guider 1.6.0 on i.MX93!     The new version has been released now, expanding to the world of MPUs! We also utilized new cloud functionality for demo examples. That means all demos are maintained and upgraded independently on application release. You can look forward to new demos during the year! It will pop out in GUI Guider instantly!     Explore the new functionality on your own https://www.nxp.com/GUI-GUIDER    
View full article
GUI Guider 1.5.1 is out now!   In this version, you can design your application much easier way by adding further features. User experience was significantly improved also as stability and performance. Checkout major updates: - Multiple instances of GUI Guider - Moving widgets between screens - 24-bit color depth for i.MX RT1170 - New demos included - and much more Try it on your own at https://www.nxp.com/GUI-GUIDER  
View full article
Hey guys   Are you interested to use RK055 LCD mounted on top of EVK? You can print LCD holders on your 3D printer, now. Only 6 screws needed. Check image and files attached.   Mike
View full article
We are pleased to announce that the v1.4.1-GA version of GUI Guider is now available! What is new   UI Development Tool Demo of video (SD) play: i.MX RT1050 Demo of runtime image (SD) decode: i.MX RT1064, LPC54S018M Non-deformation screen preview Display size of imported image Description, type, and doc link in attribute window Move editor's position with mouse Pixel scale in editor window Improved name, default value, and prompt for attributes Submenu of license Prompt of code override Auto focus on new widget in editor Improved mouse-based image rotation feature Auto-detect for custom.c and custom.h Improved robustness and stability Library Data text box widget Calendar: highlight selected date New NPI i.MX RT1040 Toolchain MCUXpresso IDE 11.6.1 MCUXpresso SDK 2.12.1 RTOS Zephyr   Installer & Documentation  https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER      
View full article
GUI Guider 1.3.0 is now available for free use on desktop systems and NXP MCU targets at the NXP website: https://www.nxp.com/gui-guider. Now MacOS users can also enjoy the benefits of the tool, joining those on Windows and Linux. Also, developers who want to work in MicroPython can output code directly from the tool and/or run simulations with the push of a button. This release of GUI Guider supports both LVGL 7.10.1 and 8.0.2, includes project creation for MCUXpresso IDE and IAR 9.10.2 and also adds support for Keil development tools (version 5.35). (Note that we will be supporting later versions of LVGL 8.x but do have to follow a little after these releases to allow for testing by our developers.) We have also added a 3D graphics animation and drag-drop tile design widget support. Full details can be found in the Release notes. As always, we encourage you to take GUI Guider for a test drive and give us any feedback at the NXP GUI Guider community space.
View full article
GUI Guider v1.2.0 is released on July 30, this video introduces key new features of the release.  IDE UI: widget search, custom font size Widget: events for list buttons, memory leak check  MCUX SDK 2.10.0, LVGL 7.10.1  Toolchain: MCUX IDE 11.4.0, IAR 9.10.2 New platform: i.MX RT1010, LPC54S018M, LPC55S69 Image converter for VGLite performance improvement  More details is available in https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER. 
View full article
GUI Guider v1.2 released (link)   The latest version of GUI Guider was recently released by NXP. GUI Guider is a user-friendly graphical user interface development tool created by NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library. GUI Guider's drag-and-drop editor makes it easy to utilize the many features of LVGL such as widgets, animations and styles to create a GUI with minimal or no coding at all.     This release of GUI Guider features: New Development Tool capabilities Search library of available LVGL widgets Specify customer font sizes Improved support and documentation of board support without relying on built-in templates New or improved Widgets Widgets and code base updated to work with LVGL 7.10.1 Improved event support Additional memory leak checking feature SDK and IDE Tool alignment Support added for direct programming and code generation for IAR Embedded Workbench Updated to align with MCUXpresso IDE 11.4.9 Updated to align with MCUXpresso SDK 2.10.x (which includes LVGL 7.10.1) HW Acceleration capabilities Image converter for VGLite performance improvement New Device Target Supported i.MX RT1010 LPC54S018M LPC55S69    
View full article