monitor.pmp file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

monitor.pmp file

Jump to solution
5,366 Views
wim_vandersteeg
Contributor II

Dear,

Application note DRM162, chapter 7 states that FreeMASTER is, and can be used for visualization of the MK34Z256VLL7 based 3-phase power meter application. Chapter 7 states as well the following:"Before running a visualization script, the FreeMASTER software must be installed on your computer. After installation, a visualization script may be launched by double-clicking on the monitor.pmp file.

The FreeMASTER software has been installed but the above mentioned monitor.pmp file cannot be found/located. For me, it seems that this is a project file for the FreeMASTER software.

Can you help me in obtaining this monitor.pmp file?

Thanks in advance and kind regards,

Wim van der Steeg

0 Kudos
Reply
1 Solution
5,268 Views
mohammad_kamil
NXP Employee
NXP Employee

@wim_vandersteeg please find the attached FreeMaster monitor.pmp file. 

View solution in original post

3 Replies
5,269 Views
mohammad_kamil
NXP Employee
NXP Employee

@wim_vandersteeg please find the attached FreeMaster monitor.pmp file. 

4,871 Views
arrivederccimamasita
Contributor III

Hi  @mohammad_kamil, 

Im having the same issue with DRM143, monitor.pmp file isn't placed. This meter have only one phase. Could I use same file as DRM162?

Tags (1)
0 Kudos
Reply
4,853 Views
mohammad_kamil
NXP Employee
NXP Employee

Hello @arrivederccimamasita, After installing DRM143, please look FreeMaster file in ".....build\iar_6_50\projects\..." under projects folder every project has its *pmp file. 

 

With Regards

Kamil