ZLG communication problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZLG communication problem

ソリューションへジャンプ
20,580件の閲覧回数
hjhjhj
Contributor IV

Hi,

    The freemaster fails to communicate with ZLG device in my computer,the ZLG device is USBCAN-II and the freemaster version is 3.0.I think my ControlCAN.dll is not the right one.Please share me a ControlCAN.dll file,which helps communication between ZLG device and freemaster .Thanks!

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 件の賞賛
返信
1 解決策
20,395件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Thanks for feedback. This new CAN plug-in version is going to be included in the upcoming 3.0.3 update.

Regards,

Michal

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
20,395件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello, can you please confirm that your ZLG CAN device can be accessed using the original CANtest software provided by ZLG? 

I have tested the FreeMASTER-ZLG compatibility using the DLL from CANtest v2.41. I'm going to re-test using the latest 2.70.

Thanks,

Michal 

0 件の賞賛
返信
20,395件の閲覧回数
hjhjhj
Contributor IV

Hi,

 Thanks for your reply!Now I open two channels in the USBCAN-II,a channel for sending messages and the other for receiving messages.It shows my ZLG CAN device works well.

pastedImage_1.png

pastedImage_2.png

Best regards!

0 件の賞賛
返信
17,639件の閲覧回数
nzola78
Contributor I

Hi

 can you help me for drivers USBCAN-II  windows 10

0 件の賞賛
返信
20,391件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I confirm that my ZLG USBCAN2 test device is also not visible, the USBCAN_2E_U device works well. 

In my case, I'm facing issues also with USBCAN2 Windows low-level driver - the device is not visible even in the CANtest so I'm not even able to test my new plugin build physically. I will try to resolve the issue as soon as possible. Anyway, I'm attaching a FreeMASTER CAN plug-in rebuilt with the latest ZLG libraries. Can you please try it on your side? Just replace the file in "c:\NXP\FreeMASTER 3.0\FreeMASTER\plugins\can" folder.

Thank you,

Michal

0 件の賞賛
返信
20,391件の閲覧回数
hjhjhj
Contributor IV

Hi,

I test it again and the ZLG USBCAN2 is still not visible.The result is  as  picture below shown.

pastedImage_1.png

Best regards!

HJ

0 件の賞賛
返信
20,391件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

I have been finally able to test this new plugin DLL with USBCAN2 device and it works well on my side. Can you make sure you have copied the DLL to the right place and that you do not have multiple FreeMASTER versions.

In case you have multiple FreeMASTER versions installed, I recommend to re-install the 3.0.2 version and copy the attached DLL to installation folder that was used for this last installation.

The properties of the DLL should show version 1.8.0.0

pastedImage_1.png

Regards,

Michal

0 件の賞賛
返信
20,391件の閲覧回数
hjhjhj
Contributor IV

Hi,

I re-install freemaster 3.0 and then replace the "focpgi.dll" in "c:\NXP\FreeMASTER 3.0\FreeMASTER\plugins\can" folder.To my surprise,it does work.Thanks very much for your help!

pastedImage_1.png

0 件の賞賛
返信
15,005件の閲覧回数
EmilyZhou8
Contributor III

I have exactly the same problem you had. I want to ask you that what file you use to replace the  "focpgi.dll" ? 

0 件の賞賛
返信
14,994件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Please make sure you are using the latest FreeMASTER version 3.2.2.2.

Regards,
Michal

0 件の賞賛
返信
20,396件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Thanks for feedback. This new CAN plug-in version is going to be included in the upcoming 3.0.3 update.

Regards,

Michal

0 件の賞賛
返信