Why the repeated data has been captured in oscilloscope function?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why the repeated data has been captured in oscilloscope function?

1,898 次查看
Dragon_J
Contributor I

The below is a part of my test data. I also selected the igore identical consecutive samples option. but still have repeated data is captured. I set the period time is 1s. the repeated data interval time is 0.002s.

I used segger J-LINK plus V11 for communication. CPU type is MKV42F64xxx16

# Oscilloscope Data

# Seconds SOCMAN_AverageCurrent_s32 SRA_OV_CalcvalCell7_st.Value_u16 SOCMAN_DisplayedStateOfCharge_u16 SOCMAN_StateOfCharge_u16
1001.154    -710    24104   163    197
1002.156    -718    24104    163   197
1003.154    -716    24096    163   197
1004.154    -720    24096    163   197
1005.154    -714    24104    163   197
1006.156    -723    24104    163   197
1007.156    -721    24104    163    197
1008.157    -714    24104    163    197
1009.157    -722    24104    164    198
1010.159    -723    24104    164    198
1011.158    -715    24104    164    198
1012.159    -719    24104    164    198
1013.160    -729    24104    164    198
1014.161    -726    24104    164    198
1015.162    -718    24113    164    198
1016.162    -715    24113    164    198
1017.162    -712    24113    164    198
1017.164    -713    24113    164    198
1018.164    -710    24113    164    198
1019.164    -707    24113    164    198
1020.163    -721    24113    164    198

0 项奖励
回复
1 回复

1,816 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

the data points you have highlighted in red are not identical. They differ at the first column. This is the reason you are getting them captured.

Regards,
Michal

0 项奖励
回复