Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.

Jump to solution
3,489 Views
matejpacha_Ineltech
Contributor II

Hi,

I just tried an upgrade from previous 3.1 version to the latest, but I'm not successful.

The installation itself is started, then it tries to remove previous version, but that is the point when it fails.

The original folder is empty (seems to be removed), I also cannot see it in the system list of installed apps, but the new installer sees it somehow (probably in registers).

Is there any way to make a clean installation, overriding the registry check? Or which registers should I "remove" before the installation starts?

Thank you,

Best regards,

Matej

0 Kudos
Reply
1 Solution
3,474 Views
iulian_stan
NXP Employee
NXP Employee

Hi @matejpacha_Ineltech,

Could you check this thread.

Hope it helps,
Iulian

View solution in original post

2 Replies
3,466 Views
matejpacha_Ineltech
Contributor II

Sorry for duplicated thread, I did search for it and did found nothing like that.

Thanks a lot!

Matej

0 Kudos
Reply
3,475 Views
iulian_stan
NXP Employee
NXP Employee

Hi @matejpacha_Ineltech,

Could you check this thread.

Hope it helps,
Iulian