S32K3x4-Q172 Serial communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3x4-Q172 Serial communication

1,500 Views
Canberk
Contributor II

When I tried to open freemaster I have got could not open the communication port error and I couldn't see my board as port as well in other serial port programs. How can I solve this problem

Thanks

Canberk_1-1675146055569.png

 

 

0 Kudos
Reply
1 Reply

1,463 Views
iulian_stan
NXP Employee
NXP Employee

Hi @Canberk,

I'm not sure I understood your issue.

  1. Does you PC correctly identify the COM port corresponding to your S32K3 board in device manager when you connect your board to the PC ?
  2. Is the UART interface used by any other application beside FreeMASTER ?
  3. What type of application are you running on the board ? Is it an example provided by NXP or your custom application ?
0 Kudos
Reply