S32K3x4-Q172 Serial communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3x4-Q172 Serial communication

1,440件の閲覧回数
Canberk
Contributor II

When I tried to open freemaster I have got could not open the communication port error and I couldn't see my board as port as well in other serial port programs. How can I solve this problem

Thanks

Canberk_1-1675146055569.png

 

 

0 件の賞賛
返信
1 返信

1,403件の閲覧回数
iulian_stan
NXP Employee
NXP Employee

Hi @Canberk,

I'm not sure I understood your issue.

  1. Does you PC correctly identify the COM port corresponding to your S32K3 board in device manager when you connect your board to the PC ?
  2. Is the UART interface used by any other application beside FreeMASTER ?
  3. What type of application are you running on the board ? Is it an example provided by NXP or your custom application ?
0 件の賞賛
返信