MPC5604B JTAG uncensoring through USB Multilink in FreeMASTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604B JTAG uncensoring through USB Multilink in FreeMASTER

2,278 Views
ginzhou
Contributor I

Hi

  I have a problem to connect MPC5604B through USB Multilink in FreeMASTER. I cannot find the option to enter JTAG password in FreeMASTER. So i tried to uncensor the device in PROGPPCNEXUS first, but it's not useful, although it's connected, but the value of variables is not correct, meaningless. XCP is disabled, so i cannot connect through CAN bus either. How can i connect a censored device in FreeMASTER?

Thank you.

Tags (3)
0 Kudos
Reply
1 Reply

2,154 Views
iulian_stan
NXP Employee
NXP Employee

Hi ginzhou‌,

Frankly speaking, we (FreeMASTER developers) never worked with censored devices. From your explanation I understand that they are password protected which implies a different connection flow or passing an additional property in the standard flow - this is not supported by the connection plugin.

Sorry for the delayed reply,

Iulian

0 Kudos
Reply