MCAT motor parameter identification (see AN4986) missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAT motor parameter identification (see AN4986) missing

1,203件の閲覧回数
HolgerMC
Contributor I

In AppNote AN4986 there is the detailed description of the motor parameter identification and the picture shows a special tab "Motor Identif".
MotorIdentif_AN4986.jpg
Even custom power boards are supported!

I want to use the S32K144 Evalboard with the DevKit MOTORGD and want to identify parameters of some unknown, small motors.
Where can this MCAT-functionality be found and which firmware is necessary to support this? Is it still available?

0 件の賞賛
返信
0 返答(返信)