Variable Watch and many other GUI issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Variable Watch and many other GUI issue

1,443 Views
Anderson_F
Contributor I

Just installing on Windows11 and I get some very small fonts in the Variable Watch section and in many other windows for configuration.

Do we have a fix for this issue?  At the moment the tools is close to not be usable.  

Is this related toa 4K monitor.  I tried on many different screen with no luck yet.

If I use the option for a "floating" windows of the Variable Watch I get a window smaller than an ICON on my desktop!!!  Not useable

Any help will be much appreciated.

0 Kudos
Reply
1 Reply

1,431 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

FreeMASTER is an typical Win32 application and all windows dimensions are given by the system. 

You can perhaps try to change the font in the Variable Watch to make at least the data grid larger, but I'm afraid the window title bar and other system parts of the windows will remain small. 

For graph views, there are some options in "Global Graph Settings" dialog which should enable to scale up the graph elements.

Can you send a screenshot of the most problematic portions of the window?

Thanks,
Michal

0 Kudos
Reply