I have MCUexpresso 11.3, FreeMASTER 3.1.1.6, a TWR-KV31F120M board and SDK 2.9 for it, a TWR-MC-LV3PH motor board. Google Chrome is my default browser. I am working with the PMSM demo program with no changes of any kind. The program starts and runs as expected, starting and stopping the motor from SW2. I have read AN4642, Motor Control Application Tuning (MCAT) Tool for 3-Phase PMSM. I have read AN4912, Tuning PMSM Sensorless Motors Using MCAT.
Based on another message here, I double click on pmsm_float.pmp, and FreeMASTER starts. From AN4912, I expect to see the NXP logo in the upper left corner, a banner header in red, two lines of tabs, a diagram labeled Application Description, and another box called Application Concept.
What I actually get is a box with Microsoft Bing in the upper left corner, and a search box preloaded with a file called StartMenu.html, a list of apparently random Google search results, and at the bottom a list of variables. If I click on the GO box, the program starts communicating with the board, and the speed variables are updated. But there are no tabs anyplace.
So how do I get tabs?
Solved! Go to Solution.
Josef and Iulian--
Success!! I unpacked SDK 2.7 to a new folder, and executed the .pmp file from there. MCAT started with all tabs showing.
Josef, when I created a project for a Tower card, it always chooses SDK 2.7, which I also had already installed.
Iulian, your suggested thread was very helpful.
Thank you both for your prompt help.
Gary
Josef and Iulian--
Success!! I unpacked SDK 2.7 to a new folder, and executed the .pmp file from there. MCAT started with all tabs showing.
Josef, when I created a project for a Tower card, it always chooses SDK 2.7, which I also had already installed.
Iulian, your suggested thread was very helpful.
Thank you both for your prompt help.
Gary
Hi Gary,
Just to clarify: TWR-KV31F120M board was supported in SDK 2.7. This board is not supported in SDK 2.9 anymore. Hopefully, I replicated the issue you are facing:
The problem is that MCUX didn't copy the MCAT content correctly to workspace (HTML pages are missing). This might be caused by some backward incompatibility (MCUX11.3 vs. SDK2.7). I don't know the real reason, you can try an older version of MCUX IDE or make a manual fix:
I recommend the easier 1) option. I hope this will help you.
Regards,
Josef
Hi @GaryOlmstead,
Could you check the following:
If there are no issues with the above it may be a IE restriction (MCAT application is using ActiveX API and needs to be run inside Internet Explorer widget as seen in point 3 above). A possible solution, in this case, is described in this thread.
Hope this helps,
Iulian
PS: let me know if none of the above works, and I will ask someone from Motor Control team to take a look at your issue.