JSON-RPC does not work in multiple FreeMASTER instances

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JSON-RPC does not work in multiple FreeMASTER instances

跳至解决方案
3,056 次查看
JaroslavP
Contributor I

Hello,

when using multiple FreeMASTER instances, only the first one is reachable using JSON-RPC. The web pages and JScript running in other instances are accessing the first running instance, similarly as other pages running standalone in a browser. I know there is a /rpcs command line option to change the JSON-RPC port, but there is no way for the HTML application to find out the port of “its” FreeMASTER instance. Or is it possible?

Thanks,

JP

0 项奖励
回复
1 解答
3,049 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello Jaroslav,

indeed, use of the /rpcs command-line option is the only way how to run multiple FreeMASTER instances each with it own JSON-RPC server. And a client script or HTML application which connects to the server needs to know the port. We realize this is not very convenient use case. This is why plan the following change in the upcoming update 3.1.3:

If started without the /rpcs option, the JSON-RPC server will automatically probe and pick a different port in range of 41001..41015 in case the default 41000 is already used. This will enable up to 16 instances to run and have their JSON-RPC servers started.

The HTML/JScript applications running inside the Chromium component embedded in the FreeMASTER main window will be able to determine the correct port. The way to achieve it is to include a "virtual" <script> file with a special URL: fmstr://localapp/info.js. This file will be supplied on-fly by the parent FreeMASTER application and will define an object with information needed to establish a JSON-RPC connection.

Please refer to "What's new" section and a User Guide of the FreeMASTER 3.1.3 when it is released by end of this month.

Thanks,
Michal

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,050 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello Jaroslav,

indeed, use of the /rpcs command-line option is the only way how to run multiple FreeMASTER instances each with it own JSON-RPC server. And a client script or HTML application which connects to the server needs to know the port. We realize this is not very convenient use case. This is why plan the following change in the upcoming update 3.1.3:

If started without the /rpcs option, the JSON-RPC server will automatically probe and pick a different port in range of 41001..41015 in case the default 41000 is already used. This will enable up to 16 instances to run and have their JSON-RPC servers started.

The HTML/JScript applications running inside the Chromium component embedded in the FreeMASTER main window will be able to determine the correct port. The way to achieve it is to include a "virtual" <script> file with a special URL: fmstr://localapp/info.js. This file will be supplied on-fly by the parent FreeMASTER application and will define an object with information needed to establish a JSON-RPC connection.

Please refer to "What's new" section and a User Guide of the FreeMASTER 3.1.3 when it is released by end of this month.

Thanks,
Michal

0 项奖励
回复