How to use the FreeMASTER to tuning touch parameters?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the FreeMASTER to tuning touch parameters?

1,280件の閲覧回数
1141886202
Contributor II

Hello,

   I want to use the example "frdmke15z_tsi_v5_selfmode" which importing from SDK2.8.0 ,but it doesn't have the FreeMASTER's function to tune  touch parameters.How should I do to porting the code about FreeMASTER from the example "frdmke15z_touch_sensing" ? I tried to copy the files and code to the project ,but it can't build successfully.

Thanks,

Yonghui Wang

0 件の賞賛
返信
1 返信

1,215件の閲覧回数
pavelrech
NXP Employee
NXP Employee

Hello,

the example "frdmke15z_tsi_v5_selfmode" is really simple example to support TSI driver only, this example does not contain the advanced touch software features like complete TSI HW configuration with selfcap and mutual mode, keydetectors, filters, controls ... and this example is not intended to be used together with FreeMASTER because there is no support of the Touch tool integrated in FreeMASTER.

It is recommended to use the frdmke15z_touch_sensing example rather supporting selfmode as well plus FreeMASTER with Touch tool together, furthermore all mentioned is tested and ready to be used. 

0 件の賞賛
返信