How to use the FreeMASTER to tuning touch parameters?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the FreeMASTER to tuning touch parameters?

1,334 Views
1141886202
Contributor II

Hello,

   I want to use the example "frdmke15z_tsi_v5_selfmode" which importing from SDK2.8.0 ,but it doesn't have the FreeMASTER's function to tune  touch parameters.How should I do to porting the code about FreeMASTER from the example "frdmke15z_touch_sensing" ? I tried to copy the files and code to the project ,but it can't build successfully.

Thanks,

Yonghui Wang

0 Kudos
Reply
1 Reply

1,269 Views
pavelrech
NXP Employee
NXP Employee

Hello,

the example "frdmke15z_tsi_v5_selfmode" is really simple example to support TSI driver only, this example does not contain the advanced touch software features like complete TSI HW configuration with selfcap and mutual mode, keydetectors, filters, controls ... and this example is not intended to be used together with FreeMASTER because there is no support of the Touch tool integrated in FreeMASTER.

It is recommended to use the frdmke15z_touch_sensing example rather supporting selfmode as well plus FreeMASTER with Touch tool together, furthermore all mentioned is tested and ready to be used. 

0 Kudos
Reply