Freemaster on CAN for s12z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster on CAN for s12z

Jump to solution
4,294 Views
tsh18609
Contributor II

Hello,

I am trying to enable Freemaster over CAN (instead of UART or BDM) on my project using the mc9s12zvmc128 device. Is this supported?

My materials:

- FreeMASTER_Serial_Communication_Driver_V2.0

- Freemaster 3.2

- IXXAT USB-to-CAN Compact device

 

0 Kudos
Reply
1 Solution
4,258 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

FreeMASTER 3.x supports all versions of communication protocol, so it is also compatible with Serial Driver 2.0 on the S12Z. FreeMASTER detects the protocol version automatically.

I don't think the new driver has been ported back to S12Z, but the example in the 2.0 driver package should work just fine.

Regards,
Michal

View solution in original post

2 Replies
4,276 Views
tsh18609
Contributor II

If I understand well: Freemaster 3.2 is not compatible with Freemaster driver V2.0, at least for the CAN (BDM and UART works well).

Where do I find FreeMASTER Communication Driver 3.0 (S12)?

0 Kudos
Reply
4,259 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

FreeMASTER 3.x supports all versions of communication protocol, so it is also compatible with Serial Driver 2.0 on the S12Z. FreeMASTER detects the protocol version automatically.

I don't think the new driver has been ported back to S12Z, but the example in the 2.0 driver package should work just fine.

Regards,
Michal