Hello NXP.
I am using S32K142 RDB and SW from below link, everything is working fine including Freemaster.
Now i am porting the same on our in-house developed HW with the processor expert configuration. below is the observation based on configuration.
1. Clock oscillator changed from 16 MHz to 8 Mhz
2. CAN is working
3. Freemaster over CAN is not working.
When the source code is compared, there is not much change concerning Freemaster.
Solved! Go to Solution.
Hi @hredekar,
Does your HW uses the same CAN instance as the RDB ? FreeMASTER uses CAN instance defined in freemaster_cfg.h, ex:
#define FMSTR_CAN_BASE 0x40025000UL /* FlexCAN1 base on S32K14x */Another thing to check is the bit rate. Considering you have different clock frequency, you may need to:
You can make a simple test to check whether FreeMASTER uses correct CAN instance by following these steps:
1. Enable polling driven communication
#define FMSTR_LONG_INTR 0 /* Complete message processing in interrupt */
#define FMSTR_SHORT_INTR 0 /* SCI FIFO-queuing done in interrupt */
#define FMSTR_POLL_DRIVEN 1 /* No interrupt needed, polling only */2. Define debug macro
#define FMSTR_DEBUG_TX 13. Connect CAN adapter and inspect the communication frames - FreeMASTER Driver should be continuously sending a test frame "+©W" (0xA9U).
Note: FreeMASTER tool won't be able to connect to the board while in debug. This test only ensures that FreeMASTER Driver is properly configured.
Hi @hredekar,
Does your HW uses the same CAN instance as the RDB ? FreeMASTER uses CAN instance defined in freemaster_cfg.h, ex:
#define FMSTR_CAN_BASE 0x40025000UL /* FlexCAN1 base on S32K14x */Another thing to check is the bit rate. Considering you have different clock frequency, you may need to:
You can make a simple test to check whether FreeMASTER uses correct CAN instance by following these steps:
1. Enable polling driven communication
#define FMSTR_LONG_INTR 0 /* Complete message processing in interrupt */
#define FMSTR_SHORT_INTR 0 /* SCI FIFO-queuing done in interrupt */
#define FMSTR_POLL_DRIVEN 1 /* No interrupt needed, polling only */2. Define debug macro
#define FMSTR_DEBUG_TX 13. Connect CAN adapter and inspect the communication frames - FreeMASTER Driver should be continuously sending a test frame "+©W" (0xA9U).
Note: FreeMASTER tool won't be able to connect to the board while in debug. This test only ensures that FreeMASTER Driver is properly configured.