FreeMaster and Ginkgo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMaster and Ginkgo

ソリューションへジャンプ
3,970件の閲覧回数
MilanBrejl
NXP Employee
NXP Employee

Can one use FreeMASTER with Ginkgo USB-CAN Interface?

http://viewtool.com/index.php/en/14-2016-07-26-07-18-35/57-2016-07-27-07-19-58 

タグ(1)
0 件の賞賛
返信
1 解決策
3,897件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Milan,

as there were more people interested in the Viewtool USB-CAN devices, we have decided to add a support to FreeMASTER version 3.0.4 (Q4/2020). Please contact me if you are interested to evaluate the support before released officially.

Regards,

Michal

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,898件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Milan,

as there were more people interested in the Viewtool USB-CAN devices, we have decided to add a support to FreeMASTER version 3.0.4 (Q4/2020). Please contact me if you are interested to evaluate the support before released officially.

Regards,

Michal

0 件の賞賛
返信
3,897件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Milan, 

no, the Viewtool/Ginkgo devices are not supported so far. Here is a list of CAN interfaces supported by FreeMASTER 3.0 (version 3.0.3):

  • IXXAT: USB-to-CAN and other compatible devices.
  • Vector: VCAN and other compatible devices.
  • National Instruments: NI-CAN and other compatible devices.
  • Kvaser: Kvaser Leaf Pro HS v2 and other compatible devices.
  • PEAK-System: PCAN-USB and other PCANBasic compatible devices.
  • GLinker: USB-CAN GY8507 and other compatible devices.
  • ZLG: USBCAN-II and other compatible devices.
  • Intrepid Control Systems: ValueCAN and other compatible devices.

Best regards,

Michal

0 件の賞賛
返信