FreeMaster GUI issue On High Resolution Screen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeMaster GUI issue On High Resolution Screen

5,062 次查看
CY9
Contributor IV

1. What is the message mean when I press [Check Title] on submit a new topic with this title :

>  Similar topics already posted
>  No matching topics found

"No matching topics found" , isn't it ?
If there exist "Similar topics", please point it out. 

CY9_0-1726712884257.pngCY9_0-1726712884257.png

 

 

2. When I preview this post, reply :

> Correct the highlighted errors and try again. 

But There is no place  HIGHLIGHTED !? 

Am I blind !?

I'd copy all message and paste it into notepad, and copy all from notepad to paste it back here.
It should be all pure text message, not exist any style code that I copy from other web page.
I don't think there exist any style error here.
Is your check code incorrect ?

CY9_1-1726712898015.pngCY9_1-1726712898015.png

 

 

3.  When I run FreeMaster on my high resolution PC, I can see NOTHING : 

CY9_2-1726713030877.pngCY9_2-1726713030877.png

 

For solve this issue, I adjust the DPI setting of thie program : 

CY9_3-1726713089930.pngCY9_3-1726713089930.png

 

This DPI setting make all graphics/text message available to see. 

BUT! 

This cause another issue: 

When I try to Export a graphics image into clipboard :

Screenshot: 

CY9_4-1726713273133.pngCY9_4-1726713273133.png

 

Actually, ONLY export this into clipboard : 

CY9_5-1726713311386.pngCY9_5-1726713311386.png

 

So, the rootcause , please try to fix resolution problem on FreeMaster app.

Thanks. 

 

 

 

 

0 项奖励
回复
5 回复数

5,037 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I do not realize I have seen any similar topic on this community.  The server engine did a wrong suggestion.

Anyway, there is a solution: In the Oscilloscope menu, select the "Global Graph Settings..." and in the dialog, try to increase relative size of the legend and other graph elements. You will need to experiment a bit with the values.

 

MichalH_0-1726726825046.pngMichalH_0-1726726825046.png

 

Regards,
Michal

 

0 项奖励
回复

5,028 次查看
CY9
Contributor IV

Dear MichalH

The  "Global Graph Settings..." already solve the font size of the oscilloscope area.

Thanks 

 

But... How about the [Variable Watch] ?

DYR: 

CY9_0-1726735939834.pngCY9_0-1726735939834.png

 

标记 (1)
0 项奖励
回复

4,987 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

In your screenshot, it seems the font in Variable Watch is scaled properly, but the rows' heights are very small. You should be able to drag the gray row sizer at the left of the grid to resize them. Select multiple cells inside the grid and then update the size for all rows.

Also, for selected cells, the toolbar controls can control the font and size like this:

MichalH_0-1727077777102.pngMichalH_0-1727077777102.png

Regards,
Michal

0 项奖励
回复

4,963 次查看
CY9
Contributor IV

No way to adjust :

CY9_0-1727085495482.pngCY9_0-1727085495482.png

 

0 项奖励
回复

4,980 次查看
CY9
Contributor IV

Dear 

Yes, It workd!

 

But this is not an easy job, so I decided to record it to show you how EASY my job is.

The screen has been enlarged x2 and speed up x1.5

0 项奖励
回复