Every RUN select device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Every RUN select device

ソリューションへジャンプ
4,314件の閲覧回数
kabron1
Contributor I

uC - Stm32F103C8

Debug probe J-link EDU mini

Every GO session begins with Device Selection dialog see picture.

It really pisses me off and makes me do not want to keep using the SW.

Is it normal?

0 件の賞賛
返信
1 解決策
4,307件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear user,

please note that use of FreeMASTER tool is permitted only with systems based on NXP central processing unit. Please stop using it with your STM device, you are violating the license conditions.

In case you would be facing a similar issue with an NXP core, please make sure to select the Core Type as CortexM0 or CortexM4/M7 in the JLink plug-in option dialog. This should be enough to help JLink driver to connect without any device prompt.

Thank you,
Michal

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,303件の閲覧回数
kabron1
Contributor I

Thanks, Michal. I took nearest to hands.

0 件の賞賛
返信
4,287件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Vladimir,

please mark the answer above as correct if it has helped to connect to NXP device without any prompts. If not, I will investigate more.

Thanks,
Michal

0 件の賞賛
返信
4,308件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear user,

please note that use of FreeMASTER tool is permitted only with systems based on NXP central processing unit. Please stop using it with your STM device, you are violating the license conditions.

In case you would be facing a similar issue with an NXP core, please make sure to select the Core Type as CortexM0 or CortexM4/M7 in the JLink plug-in option dialog. This should be enough to help JLink driver to connect without any device prompt.

Thank you,
Michal

 

0 件の賞賛
返信