CAN Calibration Protocol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN Calibration Protocol

ソリューションへジャンプ
2,393件の閲覧回数
wangyanjun
Contributor II

pcm_ug.pdf 2.5 said there are communication plug-in for CAN calibration protocol. Where can i find this plug-in? How to use it?

0 件の賞賛
返信
1 解決策
2,374件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello wangyanjun,

the last development around CAN Calibration Protocol is dated back to 2002. Indeed, we did have a plug-in which has enabled FreeMASTER to use CCP SET_MTA, UPLOAD and DNLOAD commands to access the target RAM. It has also used the ACTION SERVICE command to implement other FreeMASTER protocol services.

Later this plug-in was replaced completely by a custom FreeMASTER-over-CAN plug-in. It is not distributed and supported anymore. 

Best regards,
Michal

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,375件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello wangyanjun,

the last development around CAN Calibration Protocol is dated back to 2002. Indeed, we did have a plug-in which has enabled FreeMASTER to use CCP SET_MTA, UPLOAD and DNLOAD commands to access the target RAM. It has also used the ACTION SERVICE command to implement other FreeMASTER protocol services.

Later this plug-in was replaced completely by a custom FreeMASTER-over-CAN plug-in. It is not distributed and supported anymore. 

Best regards,
Michal

 

0 件の賞賛
返信