Bug on demo mode. Is it possible to bypass?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug on demo mode. Is it possible to bypass?

1,848 Views
Quiker
Contributor I

I found a bug on a FreeMaster configuration with the demo mode activated. If I double click on the white box of the "Variable Watch" I'm still able to add a "Watch Variable" and let it writable.

Quiker_0-1651218552646.png

 

I have the exigence to lock my FreeMaster configuration and not allow any modification on it. Is there any work around to bypass this behaviour?

Thank you very mutch.

0 Kudos
Reply
3 Replies

1,803 Views
MichalH
NXP Apps Support
NXP Apps Support

Dear Quiker,

thank you for your report. I confirm there is a gap in the demo-mode feature and it allows new watched variables to be created. It will be fixed in the new version which is to be expected by end of June. There is unfortunately no workaround.

Thanks,
Michal

0 Kudos
Reply

1,799 Views
Quiker
Contributor I

Thank you @MichalH !!!

I was able to find a workaround, but i'm glad that you will fix it!

Thanks!

Best regards.

0 Kudos
Reply

1,843 Views
PrestonSmith
Contributor I

It is configured using a local JSON configuration file which specifies the physical connection parameters, describes the ELF file to load symbols from, and also defines the Variable objects that are accessible to clients. When the service starts, it runs silently on the host computer and listens for incoming client connections.

0 Kudos
Reply