Blinky with FreeMASTER?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Blinky with FreeMASTER?

ソリューションへジャンプ
2,805件の閲覧回数
GaryOlmstead
Senior Contributor I

I have MCUXpresso 11.3.0 and SDK 2.9 for the KV31F. 

I'm watching part one of the FreeMASTER webinar, and the narrator has a demo program that is Blinky but also with FreeMASTER code.  I don't see that on my version.  The only FreeMASTER examples are a simple BDM demo and the same thing with a UART.  For the KV31F SDK, the Blinky demo does not have FreeMASTER built in, and the Import Wizard skips over the page that allows adding middle ware.

So how do you create this project?  Or did I mess up the SDK?

0 件の賞賛
返信
1 解決策
2,802件の閲覧回数
GaryOlmstead
Senior Contributor I

Never mind, I figured it out.  I missed the part where he linked FreeMASTER to Blinky by pointing it to the ELF/DWARF file.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,803件の閲覧回数
GaryOlmstead
Senior Contributor I

Never mind, I figured it out.  I missed the part where he linked FreeMASTER to Blinky by pointing it to the ELF/DWARF file.

0 件の賞賛
返信