Blinky with FreeMASTER?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Blinky with FreeMASTER?

Jump to solution
2,813 Views
GaryOlmstead
Senior Contributor I

I have MCUXpresso 11.3.0 and SDK 2.9 for the KV31F. 

I'm watching part one of the FreeMASTER webinar, and the narrator has a demo program that is Blinky but also with FreeMASTER code.  I don't see that on my version.  The only FreeMASTER examples are a simple BDM demo and the same thing with a UART.  For the KV31F SDK, the Blinky demo does not have FreeMASTER built in, and the Import Wizard skips over the page that allows adding middle ware.

So how do you create this project?  Or did I mess up the SDK?

0 Kudos
Reply
1 Solution
2,810 Views
GaryOlmstead
Senior Contributor I

Never mind, I figured it out.  I missed the part where he linked FreeMASTER to Blinky by pointing it to the ELF/DWARF file.

View solution in original post

0 Kudos
Reply
1 Reply
2,811 Views
GaryOlmstead
Senior Contributor I

Never mind, I figured it out.  I missed the part where he linked FreeMASTER to Blinky by pointing it to the ELF/DWARF file.

0 Kudos
Reply