2 Questions about Internal Community of FreeMASTER and S32K148EVB_OOBE.pmpx file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2 Questions about Internal Community of FreeMASTER and S32K148EVB_OOBE.pmpx file

Jump to solution
2,171 Views
Fumihiko_Sato
NXP Employee
NXP Employee

Hello FreeMASTER Team,


Q1. Do we have an Internal Community of FreeMASTER?
If you organize it, I would like to join it!

Q2.Do you know where I can download "S32K148EVB_OOBE.pmpx"?
Because I got a FreeMASTER Warning Message(Photo1).
I am using S32K148 below.
S32K148-Q176 Evaluation Board for Automotive General Purpose | NXP Semiconductors

I found the same as this topic for S32K146.
Solved: Getting started with S32K146EVB - NXP Community

Photo1. Warning message

Fumihiko_Sato_0-1701934410580.png


Best,
Fumi

0 Kudos
Reply
1 Solution
2,147 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello Fumi,

there is no internal community. All FreeMASTER issues are discussed publicly. You can always reach out to me if you need to discuss anything internally.

The issue you describe seems like a problem with the web address which probably got outdated. It is hardcoded in the MCU application (in one of the FreeMASTER TSA tables). I will let other users to comment on this thread.

Did you try the ZIP attached to the other "resolved" thread?

Regards,
Michal

 

View solution in original post

0 Kudos
Reply
2 Replies
2,148 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello Fumi,

there is no internal community. All FreeMASTER issues are discussed publicly. You can always reach out to me if you need to discuss anything internally.

The issue you describe seems like a problem with the web address which probably got outdated. It is hardcoded in the MCU application (in one of the FreeMASTER TSA tables). I will let other users to comment on this thread.

Did you try the ZIP attached to the other "resolved" thread?

Regards,
Michal

 

0 Kudos
Reply
2,136 Views
Fumihiko_Sato
NXP Employee
NXP Employee

Hello @MichalH Michal,

Thank you for your answer.
If I need your support, I will reach out to you.

Yes. I did the ZIP attached to the other "resolved" thread on S32K148 and it works(Photo1).
Are you planning to distribute "S32K148EVB_OOBE.pmpx" to us?

Photo1. GUI is S32K146 but MCU is S32K148.

Fumihiko_Sato_0-1702000794671.png


Best,
Fumi

 

0 Kudos
Reply