2 Questions about Internal Community of FreeMASTER and S32K148EVB_OOBE.pmpx file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

2 Questions about Internal Community of FreeMASTER and S32K148EVB_OOBE.pmpx file

跳至解决方案
1,414 次查看
Fumihiko_Sato
NXP Employee
NXP Employee

Hello FreeMASTER Team,


Q1. Do we have an Internal Community of FreeMASTER?
If you organize it, I would like to join it!

Q2.Do you know where I can download "S32K148EVB_OOBE.pmpx"?
Because I got a FreeMASTER Warning Message(Photo1).
I am using S32K148 below.
S32K148-Q176 Evaluation Board for Automotive General Purpose | NXP Semiconductors

I found the same as this topic for S32K146.
Solved: Getting started with S32K146EVB - NXP Community

Photo1. Warning message

Fumihiko_Sato_0-1701934410580.png


Best,
Fumi

0 项奖励
回复
1 解答
1,390 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello Fumi,

there is no internal community. All FreeMASTER issues are discussed publicly. You can always reach out to me if you need to discuss anything internally.

The issue you describe seems like a problem with the web address which probably got outdated. It is hardcoded in the MCU application (in one of the FreeMASTER TSA tables). I will let other users to comment on this thread.

Did you try the ZIP attached to the other "resolved" thread?

Regards,
Michal

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,391 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello Fumi,

there is no internal community. All FreeMASTER issues are discussed publicly. You can always reach out to me if you need to discuss anything internally.

The issue you describe seems like a problem with the web address which probably got outdated. It is hardcoded in the MCU application (in one of the FreeMASTER TSA tables). I will let other users to comment on this thread.

Did you try the ZIP attached to the other "resolved" thread?

Regards,
Michal

 

0 项奖励
回复
1,379 次查看
Fumihiko_Sato
NXP Employee
NXP Employee

Hello @MichalH Michal,

Thank you for your answer.
If I need your support, I will reach out to you.

Yes. I did the ZIP attached to the other "resolved" thread on S32K148 and it works(Photo1).
Are you planning to distribute "S32K148EVB_OOBE.pmpx" to us?

Photo1. GUI is S32K146 but MCU is S32K148.

Fumihiko_Sato_0-1702000794671.png


Best,
Fumi

 

0 项奖励
回复