Embedded World NXP Connectivity MCUs (RW61x, MCX W7x)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Embedded World NXP Connectivity MCUs (RW61x, MCX W7x)

ディスカッション

ソート順:
Welcome to the NXP's Embedded World FRDM Workshop!
記事全体を表示
This hands-on describes how to update the code in NBU and the User firmware using the ISP. Lab's guide: MCXW71_NBU_Firmware_Update_Using_ISP.pdf  This is the beacon example project used on this guide: frdmmcxw71_beacon_bm.zip  This is the binary file generated after building the beacon demo: beacon_frdmmcxw71_binary.zip  This is the NBU's firmware used on this Lab: mcxw71_nbu_ble_1_9_14_1.zip 
記事全体を表示
This demo shows the temperature measured from the i2c temperature sensor integrated in the board. The information can be monitored in the UART terminal or in the IoT Toolbox app. Lab's guide: FRDM-RW612_ISP_and_Temperature_sensor_over_BLE.pdf Binary required for the lab: frdm_rw612_peripheral_ht_binary.zip 
記事全体を表示
This hands-on describes how to configure FXLS8974CF accelerometer available on-board or magnetic switch sensor NMH1000 using Hall Switch 3 click expansion board on FRDM-MCXW71 to autonomously detect tampering/theft/abuse on device using low-power motion/magnetic wakeup feature and transmit ALERT message via BLE wireless UART. There are many applications where user would like to detect and be informed about damage/abuse or act of theft on their high value/secure assets at home and/or workplace environment. Target applications include Smart meters tampering, home security, Safe box/locker tampering, Personal medical device abuse, personal laptop/tablets tamper/theft, Warehouse theft detection, machine tampering, Door open/close detection etc. Lab's guide: FRDM MCXW71_Tamper_Detection_using_wakeup_sensors_over_BLE.pdf  These are the projects used on this lab:  frdmmcxw71_nmh1000_tamper_detect.zip frdmmcxw71_fxls8974_tamper_detect.zip  These are the binary files generated after building the projects used on this lab: fxls8974_tamper_frdmmcxw71_Binary.zip  nmh1000_tamper_frdmmcxw71_Binary.zip  NBU firmware used on this guide: mcxw71_nbu_ble_1_9_14_1.zip   
記事全体を表示
Getting Started using WiFi CLI demo. Lab guide: FRDM-RW612_WiFi_CLI_Getting_Started Training VS Code.pdf  If you run into any issues building the CLI example, please use this BIN file so you can give the demo a try: wifi_cli_binary.zip 
記事全体を表示
The Wi-Fi CLI (Command Line Interface) demo provides the user with a menu with different commands to explore the Wi-Fi capabilities of the FRDM RW612 board.  When the board is powered on for the first time, the green RGB LED should be blinking indicating that the demo is loaded into the board. Lab guide: FRDM RW612_OODB_Training.pdf  This ZIP file contains the files and instructions required to restore the FRDM-RW612 board to its Out of the Box state: FRDM-RW612-OOB_Demo_bin.zip 
記事全体を表示