This hands-on describes how to update the code in NBU and the User firmware using the ISP.
Lab's guide: MCXW71_NBU_Firmware_Update_Using_ISP.pdf
This is the beacon example project used on this guide: frdmmcxw71_beacon_bm.zip
This is the binary file generated after building the beacon demo: beacon_frdmmcxw71_binary.zip
This is the NBU's firmware used on this Lab: mcxw71_nbu_ble_1_9_14_1.zip
... View more
Getting Started using WiFi CLI demo.
Lab guide: FRDM-RW612_WiFi_CLI_Getting_Started Training VS Code.pdf
If you run into any issues building the CLI example, please use this BIN file so you can give the demo a try: wifi_cli_binary.zip
... View more
This demo shows the temperature measured from the i2c temperature sensor integrated in the board. The information can be monitored in the UART terminal or in the IoT Toolbox app.
Lab's guide: FRDM-RW612_ISP_and_Temperature_sensor_over_BLE.pdf
Binary required for the lab: frdm_rw612_peripheral_ht_binary.zip
... View more
The Wi-Fi CLI (Command Line Interface) demo provides the user with a menu with different commands to explore the Wi-Fi capabilities of the FRDM RW612 board. When the board is powered on for the first time, the green RGB LED should be blinking indicating that the demo is loaded into the board.
Lab guide: FRDM RW612_OODB_Training.pdf
This ZIP file contains the files and instructions required to restore the FRDM-RW612 board to its Out of the Box state: FRDM-RW612-OOB_Demo_bin.zip
... View more
The following has evaluated to null or missing:
==> coreNode.discussionStyle [in template "Language_CP_BulkTranslation_Angular" at line 35, column 37]
----
Tip: It's the step after the last dot that caused this error, not those before it.
----
Tip: If the failing expression is known to be legally refer to something that's sometimes null or missing, either specify a default value like myOptionalVar!myDefault, or use <#if myOptionalVar??>when-present<#else>when-missing#if>. (These only cover the last step of the expression; to cover the whole expression, use parenthesis: (myOptionalVar.foo)!myDefault, (myOptionalVar.foo)??
----
----
FTL stack trace ("~" means nesting-related):
- Failed at: #assign interactionStyle = coreNode.d... [in template "Language_CP_BulkTranslation_Angular" at line 35, column 9]
----
Group Hub Information
Embedded World NXP Connectivity MCUs (RW61x, MCX W7x)
FRDM-RW612, FRDM-MCXW71 Hands on WorkShop material for embedded world Austin, 2024.