WiFi stop to work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WiFi stop to work

2,111件の閲覧回数
Ratataplam
Contributor II

Hello, I'm using i.MX8 and yocto.

I found this behavior during WiFi test with Laird Connectivity Sterling LWB device.

The test is a simple "ping" from embedded device to our server.

After some hours the host become unreachable because the WiFi interfcace stop to work.

 

ifconfig 

 

shows a wlan0 with right ip address and in up/running state.

If I switch to ethenet cable the host is reachable. 

None wlan0 down->up recovery the interface and  the unique way is a board reboot.

 

In dmesg I didn't found relevant message

Someone has found a similar problem ?

Thanks

0 件の賞賛
返信
1 返信

2,061件の閲覧回数
travis-laird
Contributor I

Hi Ratataplam,

This is Travis from Laird please reach out to us at [email protected] or by going to the following page and creating a ticket at the bottom of the page. https://www.lairdconnect.com/resources/support

Thanks,

Travis

0 件の賞賛
返信