W8987 Labtool build error on Win10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

W8987 Labtool build error on Win10

1,927 Views
jodyubx
Contributor I

Dear NXP,

I downloaded labtool MFG-W8987-MF-LABTOOL-U14-1.0.0.146-16.80.205.p146.zip from website but .exe file is not available in package. I tried to build by VS2019 but got a lot of build error. I solved some but prompt more like:

Severity Code Description Project File Line Suppression State
Error MSB6003 The specified task executable "CL.exe" could not be run. System.IO.DirectoryNotFoundException: Could not find a part of the path 'C:\MFG-W8987-MF-LABTOOL-U14-1.0.0.146-16.80.205.p146\bin\labtool_app_1.0.0.146\labtool_app_1.0.0.146\Host\DutApiWiFiBt\Release\DutApiSisoBt.tlog'.
at System.IO.__Error.WinIOError(Int32 errorCode, String maybeFullPath)
at System.IO.FileSystemEnumerableIterator`1.CommonInit()
at System.IO.FileSystemEnumerableIterator`1..ctor(String path, String originalUserPath, String searchPattern, SearchOption searchOption, SearchResultHandler`1 resultHandler, Boolean checkHost)
at System.IO.Directory.GetFiles(String path, String searchPattern)
at Microsoft.Build.Utilities.TrackedDependencies.ExpandWildcards(ITaskItem[] expand)
at Microsoft.Build.Utilities.CanonicalTrackedOutputFiles.InternalConstruct(ITask ownerTask, ITaskItem[] tlogFiles, Boolean constructOutputsFromTLogs)
at Microsoft.Build.Utilities.CanonicalTrackedOutputFiles..ctor(ITaskItem[] tlogFiles)
at Microsoft.Build.CPPTasks.CL.PostExecuteTool(Int32 exitCode)
at Microsoft.Build.CPPTasks.TrackedVCToolTask.ExecuteTool(String pathToTool, String responseFileCommands, String commandLineCommands)
at Microsoft.Build.Utilities.ToolTask.Execute() DutApiSisoBt C:\Program Files (x86)\Microsoft Visual Studio\2019\Community\MSBuild\Microsoft\VC\v160\Microsoft.CppCommon.targets 687

Do we provide project files which is able to run or build for Win10?

 

Thanks.

0 Kudos
Reply
0 Replies