Questions regarding BMS: RDDRONE-BMS772

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions regarding BMS: RDDRONE-BMS772

1,711件の閲覧回数
sbi
Contributor I

Hello,

We have questions regarding the BMS: Smart Battery Management for Mobile Robotics | NXP Semiconductors for drone applications.

1. Does the device have a clock in the format year/month/day (uint8/uint8/uint8 YY/MM/DD)?

2. UAVCAN packet structure? -> We intend to connect the device to a Single Board Computer (eg Raspberry)

3. Firmware latest release BMS5.0 @GitHub: Is this version production ready or does it need additional programming? Or should we change only some values depending on our requirements in the parameters from the command line?
 
Thank you in advance.
0 件の賞賛
返信
0 返答(返信)