NXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP

1,244 Views
123Y
Contributor I

i have a problem to install the plugin Zbee pro configuration editor

with sdk JN-4141

 

the version of beyond studio  is : Build 1308

sdk jn 4170 is : Build Number 1745

I've reinstalled it twice in the default path and on D drive, and it still doesn't work.

when i install the plugin (ZB pro configuration edition 2.0.0), i have the message error :Cannot complete the install because one or more required items could not be found.

Software being installed: NXP ZBPro Configuration Editor 2.0.0 (com.jennic.sdk.zbpro.external.feature.feature.group 2.0.0)
Missing requirement: ZBPro Config Edit Support 2.0.0 (com.jennic.zps.configeditor.edit 2.0.0) requires 'bundle org.eclipse.emf.edit 0.0.0' but it could not be found
Cannot satisfy dependency:
From: NXP ZBPro Configuration Editor 2.0.0 (com.jennic.sdk.zbpro.external.feature.feature.group 2.0.0)
To: com.jennic.zps.configeditor.edit [2.0.0]

123Y_0-1680058470943.png123Y_0-1680058470943.png

 

 

0 Kudos
Reply
0 Replies