LS1028 TSN 802.1Qbu test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 TSN 802.1Qbu test

ソリューションへジャンプ
3,766件の閲覧回数
xinliwang
Contributor III

Hi, community 

When I test  ieee802.1qbu on ls1028 board, I found out the frame could not be captured by wiresharks.

Here are the setting I have done:

tc qdisc add dev eno0 root handle 1: mqprio num_tc 8 map 0 1 2 3 4 5 6 7 hw 1

tsntool qbuset --device eno0 --preemptable 0xfe

/home/root/samples/pktgen/pktgen_twoqueue.sh -i eno0 -q 0 -s 100 -n 20000 -m 90:e2:ba:ff:ff:ff

Here is the problem that I could not capture any frame from queue 1 to 7, that only 0 queue frame can be captured.

The reference menu only use "tsntool regtool 0 0x11f18" to check if the qbu is working or not. Indeed it works from my board but I wonder where do the frames go(frame from queue 1 to 7)? 

Thanks

0 件の賞賛
返信
1 解決策
3,724件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3 返答(返信)
3,751件の閲覧回数
xinliwang
Contributor III

For the TSN qbu, I have done another test;

I connect ls1028board eno0 to my PC. The eno0 ip is 192.168.0.232 and my PC ip is 192168.0.156

The ls1028 board can ping PC successfully.

Then I run the qbu command.

tc qdisc add dev eno0 root handle 1: mqprio num_tc 8 map 0 1 2 3 4 5 6 7 hw 1

tsntool qbuset --device eno0 --preemptable 0x07 

which mean I set 0 queue to preemptable.

After finish all setting, the board lose the connection with PC.

I assume the PING frame is going to queue 0 but the queue has changed to preemptable. And it only happened on eno0 port.

I wonder if this phenomenon is correct? 

I use real-time-edge v2.5 on the ls1028 board.

Thanks

0 件の賞賛
返信
3,725件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "4.1.4.1.3 Qbu" in https://www.nxp.com.cn/docs/en/user-guide/REALTIMEEDGEUG_Rev2.5.pdf.

0 件の賞賛
返信
3,720件の閲覧回数
xinliwang
Contributor III

Hi @yipingwang 

Thank you for your reply

I can not find the solution in the reference file.

My question is when I set any queues (from 0 -7) to preemptable. That queue can not send any frames any more.

For example, I set queue 0 to preemptable(tsntool qbuset --device eno0 --preemptable 0x07 ), this queue can not forward any frames even ping frame. But it is only happened on ENO0 port.

Thank you

0 件の賞賛
返信