HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1

Jump to solution
5,983 Views
vivek5676
Contributor III

Hi,

We am using i.mx9352 A1 model.

we are unable to port the BSP file due to some error is coming as given below

=======================================================

Success 0 Failure 1

 


1:2 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -f imx-boot-imx93evk-sd.bin-flash_singleboot

=============================================================================

Could you provide solution for that error

Thanks,

Vivek

 

0 Kudos
Reply
1 Solution
5,938 Views
vivek5676
Contributor III

My problem get resolved after changes done in hardware.  

View solution in original post

0 Kudos
Reply
3 Replies
5,821 Views
Binh_Hoang
Contributor II

Hi @vivek5676,

I'm facing the same issue. Could you please let me know which change is needed for this case? Please give me more details. 

Thank you in advance,

Binh

0 Kudos
Reply
5,735 Views
vivek5676
Contributor III

Hi @Binh_Hoang 

Kindly check the voltage as per Table 29 of NXP hardware design guide and check  the VDD_SOC_0V8 at SOC end.

Thanks

5,939 Views
vivek5676
Contributor III

My problem get resolved after changes done in hardware.  

0 Kudos
Reply