HALL_XOR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HALL_XOR

2,028 Views
pandi
Contributor III

IN mkv31 HALL_XOR how to detect . i trying register level if any changes and anything configure guide me help for us.

 

void initGPIO(void) {

    SIM->SCGC5 |= SIM_SCGC5_PORTB_MASK;
    PORTB->PCR[18] = PORT_PCR_MUX(3); // FTM2 channel 0
    PORTB->PCR[19] = PORT_PCR_MUX(3); // FTM2 channel 1
    PORTB->PCR[1] = PORT_PCR_MUX(3);  // FTM1 channel 1

    SIM->SCGC5 |= SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTE_MASK;
    //PORTC->PCR[6] = PORT_PCR_MUX(1); // GPIO
    //GPIOC->PDDR |= (1U << 6);        // Set as output

    //PORTE->PCR[6] = PORT_PCR_MUX(1); // GPIO
    //GPIOE->PDDR |= (1U << 6);
}




void initInputCapture(void) {
    SIM->SCGC6 |= SIM_SCGC6_FTM1_MASK | SIM_SCGC6_FTM2_MASK;
    FTM1->MODE |= FTM_MODE_WPDIS_MASK;
    FTM2->MODE |= FTM_MODE_WPDIS_MASK;

    FTM1->MOD = 0xFFFF;
    FTM2->MOD = 0xFFFF;
        FTM2->COMBINE |= FTM_COMBINE_DECAPEN0_MASK; // Assuming this enables XOR on FTM2 CH0 and CH1
          SIM->SOPT4 |= SIM_SOPT4_FTM2CH1SRC_MASK;
    FTM2->CONTROLS[0].CnSC = FTM_CnSC_CHIE_MASK | FTM_CnSC_ELSA_MASK;
    FTM2->CONTROLS[1].CnSC = FTM_CnSC_CHIE_MASK | FTM_CnSC_ELSA_MASK;
    FTM1->CONTROLS[1].CnSC = FTM_CnSC_CHIE_MASK | FTM_CnSC_ELSA_MASK;
    FTM2->SC |= FTM_SC_TOIE_MASK;
    FTM1->SC |= FTM_SC_TOIE_MASK;
    NVIC_EnableIRQ(FTM2_IRQn);
    NVIC_EnableIRQ(FTM1_IRQn);

    FTM2->SC = FTM_SC_CLKS(1) | FTM_SC_PS(0);
    FTM1->SC = FTM_SC_CLKS(1) | FTM_SC_PS(0);
}


void FTM2_IRQHandler(void) {

	if (FTM2->SC & FTM_SC_TOF_MASK) {
	        FTM2->SC &= ~FTM_SC_TOF_MASK; // Clear the overflow flag
	        GPIO_PortToggle(GPIOC, 1U << 6); // Example: Toggle GPIOC pin 6 for overflow visualization
	    }
    if(FTM2->CONTROLS[0].CnSC & FTM_CnSC_CHF_MASK) {
        GPIO_PortClear(GPIOC, 1U << 6);
        a+=b;
        FTM2->CONTROLS[0].CnSC &= ~FTM_CnSC_CHF_MASK; // Clear flag
        GPIO_PortClear(GPIOC, 1U << 6);
    }
    if(FTM2->CONTROLS[1].CnSC & FTM_CnSC_CHF_MASK) {

        GPIO_PortClear(GPIOC, 1U << 6);
        FTM2->CONTROLS[1].CnSC &= ~FTM_CnSC_CHF_MASK; // Clear flag
        GPIO_PortClear(GPIOC, 1U << 6);
    }
    GPIO_PortClear(GPIOC, 1U << 6);
}


void FTM1_IRQHandler(void) {
    // Handle input capture for FTM1 CH1
    if(FTM1->CONTROLS[1].CnSC & FTM_CnSC_CHF_MASK) {
        GPIO_PortClear(GPIOE, 1U << 6);
        FTM1->CONTROLS[1].CnSC &= ~FTM_CnSC_CHF_MASK; // Clear flag
        GPIO_PortClear(GPIOE, 1U << 6);
    }
}

 

                                          Thankyou

BR

PANDI

0 Kudos
Reply
1 Reply

1,988 Views
pandi
Contributor III

HI

Every one if anyone know how to configure HALL SENSOR_XOR method in mkv31f512vll12?

0 Kudos
Reply