CodeWarrior 11.1 Can't find SmartLinker Detailed Warning Messages Manual

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior 11.1 Can't find SmartLinker Detailed Warning Messages Manual

跳至解决方案
1,711 次查看
BooleanBob
Contributor IV

Using HCS08 MCU's I have downloaded a lot of CodeWarrior manuals in PDF format from the NXP site. Many of them contain a partial content about the use of the SmartLinker, as if the information for the Linker is scattered among the Compiler and other tools.

In the case of messages like:

WARNING L1823: External object x in D:/DATA/WorkspaceJavier/Extern/FLASH/Sources\Mod1_c.obj created by default

I need the specific and complete SmartLinker manual, and as I can remember, this manual existed since the old MeteoWerks CodeWarrior 6.3 version, an also I can remember a complete and detailed listing for the compiler Cxxxx messages and the Lxxxx linker messages aswell.

Could somebody please indicate a link for downloading this particular complete and detailed SmartLinker for CW 11.1 manual?

Thank you in advance,

 

0 项奖励
回复
1 解答
1,702 次查看
ErichStyger
Specialist I

It is installed and present for me here:

ErichStyger_0-1672765330817.png

 

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,691 次查看
BooleanBob
Contributor IV

Thank you Eric, you are right, I got confused with the names of the several manuals, I was wrongly looking here:

CodeWarrior V10.x RS08 Build Tools Reference Manual CWMCURS08CMPREF

CodeWarrior V10.x HC(S)08 Build Tools Reference Manual CWMCUS08CMPREF

The right manual has this title:

CodeWarrior V10.x HC(S)08 RS08 Build Tools Utilities Manual

All the linker messages are there in detail.

Now I can write a new post with a problem based on this reference.

Thank you !

 

 

1,703 次查看
ErichStyger
Specialist I

It is installed and present for me here:

ErichStyger_0-1672765330817.png

 

I hope this helps,

Erich

0 项奖励
回复