CodeWarrior 11.1 Can't find SmartLinker Detailed Warning Messages Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior 11.1 Can't find SmartLinker Detailed Warning Messages Manual

ソリューションへジャンプ
2,646件の閲覧回数
BooleanBob
Contributor IV

Using HCS08 MCU's I have downloaded a lot of CodeWarrior manuals in PDF format from the NXP site. Many of them contain a partial content about the use of the SmartLinker, as if the information for the Linker is scattered among the Compiler and other tools.

In the case of messages like:

WARNING L1823: External object x in D:/DATA/WorkspaceJavier/Extern/FLASH/Sources\Mod1_c.obj created by default

I need the specific and complete SmartLinker manual, and as I can remember, this manual existed since the old MeteoWerks CodeWarrior 6.3 version, an also I can remember a complete and detailed listing for the compiler Cxxxx messages and the Lxxxx linker messages aswell.

Could somebody please indicate a link for downloading this particular complete and detailed SmartLinker for CW 11.1 manual?

Thank you in advance,

 

0 件の賞賛
返信
1 解決策
2,637件の閲覧回数
ErichStyger
Specialist I

It is installed and present for me here:

ErichStyger_0-1672765330817.png

 

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,626件の閲覧回数
BooleanBob
Contributor IV

Thank you Eric, you are right, I got confused with the names of the several manuals, I was wrongly looking here:

CodeWarrior V10.x RS08 Build Tools Reference Manual CWMCURS08CMPREF

CodeWarrior V10.x HC(S)08 Build Tools Reference Manual CWMCUS08CMPREF

The right manual has this title:

CodeWarrior V10.x HC(S)08 RS08 Build Tools Utilities Manual

All the linker messages are there in detail.

Now I can write a new post with a problem based on this reference.

Thank you !

 

 

2,638件の閲覧回数
ErichStyger
Specialist I

It is installed and present for me here:

ErichStyger_0-1672765330817.png

 

I hope this helps,

Erich

0 件の賞賛
返信