Programming FMUK66 for first use

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming FMUK66 for first use

ソリューションへジャンプ
4,749件の閲覧回数
ArifKamal
Contributor I

My RDDRONE-FMUK66 board could not connect using the debugger given by the it. As i was following the gitbook step by step, im stuck at the bootloader part. When using Jlink Commander in Windows and trying to connect MK66FN2M0xxx18 through SWD as the target interface, it gives out a response "cannot connect to target" why is that? can anybody help me?

Screenshot 2021-06-10 040949.png

 

ラベル(2)
0 件の賞賛
返信
1 解決策
4,736件の閲覧回数
dk7xe
Contributor II

You need to power up the FMU via USB or the included power module to be able to program it.

元の投稿で解決策を見る

2 返答(返信)
4,737件の閲覧回数
dk7xe
Contributor II

You need to power up the FMU via USB or the included power module to be able to program it.

4,726件の閲覧回数
ArifKamal
Contributor I

Thank you very much

0 件の賞賛
返信