mc56f8367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc56f8367

2,469 次查看
sasikumar_e
Contributor II

hi i am new to embedded programming i like to program a bldc motor with mc56f8367 with IDE

CodeWarrior® Development Studio for 56800/E Digital Signal Controllers (Classic IDE) v8.3

but i m unable to find header files for the particular microcontroller and i am using a 64 bit windows 7 os and there some progress to be taken for the perfect functioning of codewarrior, is there any other version that support 64 bit Windows 7, containing header files or any other way to download header files

0 项奖励
回复
4 回复数

2,142 次查看
padmaashok765
Contributor II

Hi,

I am using codewarrior v8.3 to program mc56f8367. I need default header file for it.

Thanks in advance

0 项奖励
回复

2,142 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Padma,

I attach the header file for MC56F8367, hope it can help you.

BR

Xiangjun Rong

0 项奖励
回复

2,142 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Kumar,

I suggeat you use MC56F84xxx and MC56F82xxx, they are new product.

Digital Signal Controllers | NXP 

The MC56F83xx is a bit old.

Currently, both the CodeWarrior for DSP56800E ver8.3 and CodeWarrior for MCU ver11 support the MC56F83xx, both can be installed on the Win7 bit64 and Win10 bit 64 OS.

Regarding the peripheral header file, which includes the peripheral address, it is dependent on the processor itself and whether you use PE, anyway, the header file is available.

This is the example code:

56F836X-816X|Digital Signal Controllers | NXP 

Hope it can help you

BR

XiangJun Rong

2,142 次查看
Ben
Senior Contributor I

Hello,

I apologize that I have to remark, as you are  NXP stall engineer and probably have more experience than me. But I have to say that the 8.3  debugger did not work good for me on the 8367 (windows7).

Several years ago I started working with eclipse version, and it works good for all the DSC family

Ben

0 项奖励
回复