i am getting this message from the code warrior when i start debugging( MC56f8257 DSC and codewarrior ide v5.6)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i am getting this message from the code warrior when i start debugging( MC56f8257 DSC and codewarrior ide v5.6)

3,250件の閲覧回数
akshaykatkar
Contributor I

11201_11201.pngCapture1.PNG.png

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,091件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

I suspect that you select the incorrect *.cfg file, which is used for CW to download code/data to flash in downloading process. This is the procedure based CodeWarrior for DSP56800/E ver8.3:

1)On CW IDE, pls press "ALT" plus "F7" button, the "smm pROM-xRAM settings" menu will appear.

2)click "Debugger->M56800E Target Setting", the "M56800E Target Settings" will appear.

3)check "Use Initialization file" box, select "56825x_flash.cfg", if the box is empty, pls click "Choose" button to select correct one in the directory:

C:\Program Files\Freescale\CodeWarrior for DSC56800E v8.3\M56800E Support\initialization

0 件の賞賛
返信

3,091件の閲覧回数
akshaykatkar
Contributor I

the  Initialization file, "56825x_flash.cfg" was present but still it didn't work. when i tired debugging in simulator mode it was displaying an unknown program is running.

0 件の賞賛
返信

3,091件の閲覧回数
akshaykatkar
Contributor I

Thank you i will try

On Wed, Apr 23, 2014 at 12:15 PM, xiangjun.rong <

0 件の賞賛
返信