codewarrier

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrier

3,244 Views
Ujwala_kontham
Contributor I

while Iam trying to debug in CodeWarrior IDE using Multilink LC debug probe, getting the below error

Ujwala_kontham_0-1705985737580.pngUjwala_kontham_0-1705985737580.png

please get me solution to resolve this.

0 Kudos
Reply
4 Replies

3,226 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Do you use CodeWarrior for MCU ver11.x tools and Multilink Universal device? what is the part number you are using?

Pay attention to the pin 1 of the 14 pins JTAG connector, the red line of flat cable is cable 1.

BR

XiangJun Rong

0 Kudos
Reply

3,216 Views
Ujwala_kontham
Contributor I

Yes, Iam CodeWarrior for MCU ver11.x tools and am using Multilink Universal REV E (PEM9D3DA6) debugger and MC56F82746 uc and did correct connection as mentioned

0 Kudos
Reply

3,211 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

if you insert USB port, can you see the USB icon on the PC device manager?

I have tried to connect the multilink Universal with MC56F83000-EVK, no problem.

This is the device manager of PC

xiangjun_rong_0-1706087331376.pngxiangjun_rong_0-1706087331376.png

 

BR

XiangJun Rong

0 Kudos
Reply

3,210 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

On the Multilink Universal device, you have to connect the 14 pin PORT A JTAG/ONCE connector.

BR

XiangJun Rong

0 Kudos
Reply