Write endurance for the MC56F847XX Program Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write endurance for the MC56F847XX Program Flash

2,321 Views
EngHuiPeng
NXP Employee
NXP Employee

What is the  write endurance for the MC56F847XX Program Flash? Is it 10K cycles? Is there any register that could read on the no. of write cycles. Thanks.

Labels (1)
0 Kudos
Reply
3 Replies

2,037 Views
EngHuiPeng
NXP Employee
NXP Employee

XiangJun,

Do we have any application examples that Customer could push to the max of the write/read to do testing on their reliability?

Thanks.

Regards,

Audrey

0 Kudos
Reply

2,038 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Audrey,

The reliability specs of flash in data sheet is provided by test team, as AE engineers, we do not have the test code to test the max of reading and writting.

sorry for not helping you.

BR

Xiangjun Rong

0 Kudos
Reply

2,038 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

HI,

The minimum cycles of erasing and programming for MC56F847xx flash is 10K, the maximum is 50K.

I copy the specs from the data sheets:

Hope it can help you.

BR

XiangJun Rong

pastedImage_0.png

0 Kudos
Reply