Using the PN5180 with Balun

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the PN5180 with Balun

1,213件の閲覧回数
berndbogenriede
Contributor I

Good Morning Guys,

in a new little project we want to use the PN5180 with a extended antenna. This should be realized over a Balun after the EMC network.

We found some examples which are really helpfully for using the CLRC663 because it only has one RX Pin. But what should we do with the second Rx Pin of the PN5180? is there a register to use both or is it only regulated by the AGC (Page 79 in the Datasheet).

Wish you a wonderful day :smileyhappy:

タグ(2)
0 件の賞賛
返信
0 返答(返信)