Does AUX channel of Displayport need to be length matched to main link lanes?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does AUX channel of Displayport need to be length matched to main link lanes?

2,063 次查看
ludwigbrechter
Contributor I

Dear community,

I am currently designing a PCB containing multiple Displayport/HDMI muxes. I want to achieve at least achieve  HBR2 (5.4Gbit/s/lane), better even HBR3 (8.1Gbit/s/lane).

Here a signal overview from Wiki:

DisplayPort pinsDVI/HDMI mode
Main Link Lane 0TMDS Channel 2
Main Link Lane 1TMDS Channel 1
Main Link Lane 2TMDS Channel 0
Main Link Lane 3TMDS Clock
AUX CH+DDC Clock
AUX CH−DDC Data
DP_PWRDP_PWR
Hot Plug DetectHot Plug Detect
Config 1Cable Adaptor Detect
Config 2

CEC (HDMI only)

During layout I have considered "AN10798".

It says: "Trace length greatly affects the loss and jitter budgets of the interconnection. The PCB trace may introduce 1 ps to 5 ps of jitter and 0.35 dB to 0.50 dB of loss per inch." 

For 1ps and 300.000.000m/s speed (I know it is a bit slower on PCB) it equals to roughly 0,3mm. With 200.000.000m/s and 5ps it still means 1mm. That is fine for the 4 main lanes but aux channel makes it a bit harder in my application.

Now I am wondering, if length matching is only important between the four lanes of main link so aux channel can be of another length (which would give me great freedom in layout) or if the aux pair needs to be within same 0.3~1mm length matching as stated in AN10798.

Just to be clear, I know, that p and n signal needs to be same length, but does the diff pair need to be the same length as the four main link diff pairs?

Thank you very much for your help!

标签 (1)
0 回复数