Using the PN5180 with Balun

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the PN5180 with Balun

1,229 Views
berndbogenriede
Contributor I

Good Morning Guys,

in a new little project we want to use the PN5180 with a extended antenna. This should be realized over a Balun after the EMC network.

We found some examples which are really helpfully for using the CLRC663 because it only has one RX Pin. But what should we do with the second Rx Pin of the PN5180? is there a register to use both or is it only regulated by the AGC (Page 79 in the Datasheet).

Wish you a wonderful day :smileyhappy:

Tags (2)
0 Kudos
Reply
0 Replies