Dear Xiangjun Rong;
CW 8.3 supports the USBDM, see photo, and is
running well.
The problem is with version _200 of USBDM, the older
version _140 runs.
BR,
Paulo R L Barbosa
Nova PRecursor
Industria,
Comércio e Serviços
27 Anos 1990-2017
Av João Carlos da Silva Borges
873 Sala 2
04726-001 São Paulo SP
(11)2337-1591
Skype NovaPRecursor
Em
04.08.2017 02:33, xiangjun.rong escreveu:
NXP COMMUNITY
RE:
USBDM IS NOT RUNNING WITH MC56F
reply from xiangjun.rong in
Digital Signal Controllers - View the full discussion
>