USBDM is not running with MC56F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USBDM is not running with MC56F

4,069 次查看
pauloprecursor
Contributor I

I´m trying to use USBDM with MC56F8006. Inside CW 8.3 it works, but the stand alone MC56F Programmer software is not working. Ex., trying to Mass Erase the dsc, always returns the message "Execution of TCL script returned an error".

Somebody can help ? It is USBDM-JMxx-CF-0001.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

3,478 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Paulo,

Unfortunately, the "56800E Flash Programmer" tools does not support USBDM interface, you have to use USBTAP device to download the code/data to flash.

BR

Xiangjun Rong

pastedImage_1.png

0 项奖励
回复

3,473 次查看
pauloprecursor
Contributor I

Dear Xiangjun Rong;

CW 8.3 supports the USBDM, see photo, and is

running well.

The problem is with version _200 of USBDM, the older

version _140 runs.

BR,

Paulo R L Barbosa

Nova PRecursor

Industria,

Comércio e Serviços

27 Anos 1990-2017

Av João Carlos da Silva Borges

873 Sala 2

04726-001 São Paulo SP

(11)2337-1591

Skype NovaPRecursor

Em

04.08.2017 02:33, xiangjun.rong escreveu:

NXP COMMUNITY

RE:

USBDM IS NOT RUNNING WITH MC56F

reply from xiangjun.rong in

Digital Signal Controllers - View the full discussion

>

0 项奖励
回复

3,473 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Paulo,

Yes, the CodeWarrior for DSP56800E ver8.3 supports USBDM, but  the "56F800E Flash programmer" tools does not support USBDM.

BR

xiangjun rong

0 项奖励
回复